The SMA Miniature S-Type Load Cells are inserted into the line of the cheekpiece and reins on one side of the horse. The SMA Miniature S-Type Load Cells are resistive wire strip strain gages whose changes in potential difference, produced with strain, are transferred to transmitters which send the data by the BTS Bluetooth® Telemetry System to a receiver connected to a USB port of a PC.
The BTS-AM-1 Bluetooth® Low Energy (BLE) Strain Bridge Transmitter Modules are held inside modified camera cases attached to a breastplate on the horse. The rider is therefore not carrying any of the electrical equipment. Before the data is collected and after the cheekpiece is pretensioned, the SMA Miniature S-Type Load Cells are tared to zero.
This makes it possible in some cases to see negative net values for cheekpiece tension when rein tension is applied to the cheek. The rider takes a normal contact on both reins and performs ridden exercises in the three lower gaits, and the natural resistive counter-contact from the body of the horse provides pairs of force data from the rein and cheekpiece. Because the cheekpiece is directly attached to the headpiece, we can assume that forces seen in the cheekpiece are those that are applied to the poll of the horse.